Mixer Selection (External Mixer)

The Mixer Selection drop-down menu allows you to select a predefined external mixer type and band, which configures the Harmonic Table automatically. You can also set up a Custom (single harmonic) mixer configuration.

USB Smart Mixers

When a supported smart mixer is plugged into the USB port of the X-Series Signal Analyzer, the VSA will automatically set the Mixer Selection to the smart mixer and populate the Harmonic Table and the USB Mixer status area with the information for the smart mixer.

The amplitude corrections supplied by the smart mixer to the X-Series Analyzer will be applied to the time data sent to the VSA.

See Also

USB Mixer Status

Harmonic Table

External Mixer tab