Control Toolbar
The Control toolbar provides quick access to the main selections under the Control menu:
These operations affect the selected measurement.
|
Starts a measurement or restarts one that was paused. Click this button and all current measurement data (including averaging) is discarded. |
|
|
Pauses a running measurement. A second click then single steps (when Sweep is set to ) or continues the measurement (when is set to ). |
|
![]() ![]() |
Single/Continuous Sweep | Switches between single or continous sweep mode. |
![]() |
Auto-range |
Performs an auto-range of all input channels for the Analyzer Configuration of the selected measurement and restarts the measurement. Click the dropdown part of the button to perform an autorange on a specific input channel. |