Matrix Tables
Measurement software options may provide matrix tables to display and sort various statistical data.
Copying/Pasting and Exporting Matrix Table Data
Querying Matrix Table Data Results Programmatically
Column Operations
With matrix tables, you can right-click the column header to display a menu with the following choices:
- Preset Columns -- returns all columns to their default widths and visibility, and displays only the default set of columns.
- Clear Sort -- turns off sorting (you can sort a column by clicking any column header).
- Undo -- undoes the last operation.
- Redo -- repeats the last operation.
- Optimize Table -- The Pulse Table (Pulse Analysis option) and FMCW Region Table (FMCW Radar Analysis option) provide a choice between optimizing large tables for speed and responsiveness or for sortability.
- Column Visibility -- displays a list of available columns that you can select or deselect, allowing you to choose which columns appear in the matrix table.
Sorting Data
You can sort the metrics in the Pulse Table by clicking any column header. For example, to sort the Droop metrics in ascending order, click the Droop (dB) column label. To undo the sort, right-click the column label and select Clear Sort.
Not every matrix table supports sorting. Some measurements disable sorting for a particular table; in that case clicking a column header does not reorder the rows, no sort indicator appears, and the Clear Sort command is not available.
Optimize Table
The Pulse Table (Pulse Analysis option) and FMCW Region Table (FMCW Radar Analysis option) provide a choice between optimizing large tables for speed and responsiveness or for sortability.
- Speed & Responsiveness (Default) -- This selection optimizes the table for maximum responsiveness. However, tables cannot be sorted while a measurement is running continuously.
- Sortability While Running -- This selection allows sortability while the measurement is running continuously. However, this selection can make the UI less responsive for tables with a large number of rows.
Column Visibility
You can choose which metrics (columns) to display in the matrix tables, as follows:
To return all columns to their default widths and display only the default set of columns, right-click any column label and select Preset Columns.
You can change the width of columns by dragging the right boundary of the column header.
Changes in column width or visibility can be reverted by undo, or restored by redo.
-
Right-click any column label (heading)
-
Select Column Visibility
-
In the Column Visibility dialog, check the metrics you want displayed in the table, then click OK.
You can also right-click and select Preset Columns to display the default column set.
Row Operations
In matrix tables, you can also select a range of cells and right-click to perform the following operations:
- Copy -- copies the selected data to the clipboard. This technique provides an easy way to copy data into other applications, such as Excel.
- Select All -- selects all data in the matrix table.
Copying/Pasting and Exporting Matrix Table Data
Any or all rows in a matrix table can be copied and pasted into email, text editing or spreadsheet programs for communication or further analysis. To do this, use your mouse as follows:
- To copy a single row:
- Click the Row, then right-click > Copy and paste the row into the external program.
- To copy all rows:
- Click any row, then right-click > Select All, right-click> Copy and paste the entire set of rows into the external program.
- To copy a range of rows:
- Click the first row, press the Shift key, click the last row, then right-click > Copy and paste the rows into the external program.
- To copy multiple random rows:
- Press the Ctrl key and left-click the rows that you want to copy, then right-click > Copy and paste the rows into the external program.
- To export the trace data to .csv or .txt format:
- Select the trace, then click File > Export Trace and select the desired format.
Querying Matrix Table Data Results Programmatically
Matrix table results are row-based. To get values in a row programmatically, use the row index (0-n). The row index can be determined by looking at the trace's default row order. The top row has a row index of 0, the next row has an index of 1, and so on. You can also determine a row's index programmatically by putting together enough of a table's identifiers (PhysicalChannel, PhysicalChannelPart, Layer, PhysicalChannelIndex, etc.) to distinguish the desired row from other rows.