Cross Spectrum (Trace Data)
trace data (also called cross power spectrum) is a two-channel measurement. Cross spectrum is seldom used as a separate measurement, but is used internally by the VSA to compute other measurements such as transfer function and Coherence.
This trace data is available only when more than a single input channel is selected.
The cross spectrum, Gxy, is defined as taking the FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. of two signals separately and multiplying the results together, as follows:
The exact computation used by the VSA depends on the type of average used:
|
If the average is: |
the VSA uses this formula: |
|---|---|
|
None |
A |
|
Time |
A |
|
Time exponential |
A |
|
rms |
B |
|
rms exponential |
C |
|
peak hold/continuous peak hold |
cross spec. unavailable |
|
Term |
Definition |
|---|---|
|
L |
number of averages |
|
linspec,N |
linear spectrum channel N |
|
xavg |
(1/L) * new + ((L-1)/L)* old |
|
conj |
conjugation |