Inst Main Time (Trace Data)

Inst Main Time shows the instantaneous time-domain data for the selected input channel.

The following block diagram shows how Instantaneous Main Time is derived. This is a portion of the VSA Block Diagram.

 

Notice that Instantaneous Main Time shows time data before time averaging. If time averaging is off, Instantaneous Main Time is identical to Main Time.

Inst Main Time is only available when time gating is available (in the Vector and Analog Demod measurement types).

See Also

Main Time