Window Shapefactor and Equivalent Noise Bandwidth
The following table shows a performance summary of the different types of windows supported by the 89600 VSA. Following the table is a section that describes the terms shapefactor and equivalent noise bandwidth.
Window Shapefactor & Equivalent Noise Bandwidth
Window shapefactor is a frequency ratio. It is the ratio of the frequency at -3dB to the frequency at -60dB. Window shapefactor is sometimes called window selectivity.
Equivalent noise bandwidth (ENBW) compares a window to an ideal, rectangular time-window. It is the bandwidth of the rectangular window's frequency-domain shape that passes the same amount of white noise energy as the frequency-domain shape defined by the other window.
In the table below, the ENBW has been normalized by the time-record length. To compute the ENBW for a given time-record length, divide the ENBW by the time-record length. For example, a Hanning window on a 0.5 second time record would have an ENBW of 3 Hz (1.5 Hz-sec/0.5 sec). Notice that the ENBW is slightly larger than the 3 dB bandwidth.
The VSA's definition of resolution bandwidth (ResBW) is based on the normalized Equivalent Noise Bandwidth of the selected window type.
|
Parameter |
Uniform |
Hanning |
Gaussian Top |
Flat Top |
|---|---|---|---|---|
|
Leakage Performance |
Poor |
Relatively Good |
Best |
Good |
|
Frequency Resolution: main length fixed |
Poor** |
Relatively Good |
Good |
Poor |
|
Poor** |
Good |
Good |
Best |
|
|
Normalized Equivalent Noise BW |
1.00 Hz-sec |
1.50 Hz-sec |
2.215 Hz-sec |
3.8194 Hz-sec |
|
3 dB BW |
0.8844 Hz-sec |
1.438 Hz-sec |
2.091 Hz-sec |
3.767 Hz-sec |
|
Window ShapeFactor |
716:1 |
9.1:1 |
4.0:1 |
2.45:1 |
|
Maximum Amplitude Error* |
3.92 (dB) |
1.42 (dB) |
0.68 (dB) |
< 0.01 (dB) |
|
Highest Sidelobe |
-13 (dB) |
-31 (dB) |
-125 (dB) |
-95 (dB) |
|
Sidelobe Fall Off |
-20 dB / decade |
-60 dB / decade |
-20 dB / decade |
-20 dB / decade |
|
Parameter |
Blackman-Harris |
Kaiser-Bessel |
Gaussian |
|---|---|---|---|
|
Leakage Performance |
Good |
Good |
Good |
|
Frequency Resolution |
Good |
Good |
Good |
|
Normalized Equivalent Noise BW |
2.0044 Hz-sec |
2.0013 Hz-sec |
2.0212 Hz-sec |
|
Window ShapeFactor |
3.79 |
3.78 |
4.45 |
|
Maximum Amplitude Error* |
0.83 (dB) |
0.83 (dB) |
0.83 (dB) |
|
Highest Sidelobe |
-92 (dB) |
-89 (dB) |
-73 (dB) |
|
Sidelobe Fall Off |
-20 dB / decade |
-20 dB / decade |
-20 dB / decade |
|
* |
The maximum amplitude error occurs when a signal is halfway between frequency bins. |
|
** |
Frequency resolution is best for equal amplitude signals (for example, two closely spaced sine waves) but poor in general because of the large sidelobes. |