Symbol Table Format (Digital Demod)
The Symbol Table. The available format choices are binary or hexadecimal formats:
specifies the format used to display the symbol binary bit data in theBinary Format: The symbol data bit format is binary and each character represents a binary digit. The number to the left of each row indicates the bit offset of the first bit in the row.
Hexadecimal Format: The symbol data bit format is hexadecimal and each character represents a hexadecimal digit. The number to the left of each row indicate the symbol offset of the first symbol in the row.
There must be at least 4 bits/symbol to use the hexadecimal format, that is, symbols that have less than 4 bits/symbol will only be displayed in binary format regardless of the
settingThis parameter is valid only when the active trace is a symbol table.
See Also