Zoom If Span Change (Frequency)
determines whether Time Data is switched to mode (complex samples) when the is changed in mode (real samples). Note that in mode, the frequency is always 0 Hz.
When is selected, changing the will adjust the and frequencies to center the desired around the current frequency. This causes the frequency to change from 0 Hz, causing Time Data to switch to mode.
However, when is cleared and the is changed, the frequency will remain at 0 Hz and only the frequency will be adjusted to reach the desired . This also means that the frequency will change when you adjust the .
The following picture illustrates the effect of this parameter when changing the span.
See Also