Frequency Unit (Digital Demod)
selects the x or z-axis frequency units that are applied to marker readouts for trace data results that use carrier information. The available measurement units are carrier or Hz.
For example, z-axis marker readouts for digital demodulation trace data can be viewed in units of carrier or Hz.
This parameter is not applicable to certain demodulators such as Opt. B7T cdma2000/1xEV-DV and Opt. AYA Digital Demodulation.
See Also