Time Unit (Digital Demod)
selects the x- or z-axis Time units that are applied to marker readouts for trace data results that use symbol information. The available measurement units are sym (symbols) or sec (seconds).
For example, view the trace data symbol locations for an EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.) demodulated signal in units of symbols or time.
Exception
For and demodulation the x-axis symbol unit is replaced with chip for marker readouts using the trace data.
See Also