Changing Frequency Settings

The settings for frequency parameters can be changed in several ways:

  1. From the Frequency Tab:

    1. Click Analysis > Frequency.

    2. To set Center Frequency or Frequency Span, be sure that the Show Center/Span check box is selected. To set Start or Stop Frequency, be sure that the Show Center/Span check box is cleared.

    3. Click the parameter to change (for example, Center).

    4. Type the new value and press Enter or click Close.

  2. From the Copy Marker to menu:

    Click Markers > Copy Marker to, and the appropriate selection from the menu (Copy Mkr to Center Freq, for example).

  3. From the Trace popup menu

    1. Right-click in the trace.

    2. From the popup menu, click Copy Mkr to Center Freq.

  4. Using the Select Area tool

    1. Click the Select Area tool.
    2. Draw a box around the frequency band of interest.
    3. From the popup menu, click the appropriate selection (for example, Frequency Center and Span).