External Reference Frequency (Frequency Reference)
The specifies the frequency of the external reference signal. Valid entries depend on the hardware the reference signal is connected to.
When the System Reference Instrument is changed, the VSA resets the External Reference Frequency to 10 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. for all other measurement hardware.
See Also