Multi-Channel Measurements (Input Channels)
The 89600 VSA software supports multi-channel measurements from multi-channel hardware. For example, a 4 channel MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. measurement using a 4 channel oscilloscope. The number of available measurement input channels is determined by the measurement hardware input channels.
For best measurement speed, only use the number of channels required for the measurement.
See Also