% Power (OBW Markers Tab)
: cleared
: 0% to 100%
The frequency span to capture with the OBW Occupied bandwidth is closely related to channel power. It indicates how much frequency spectrum is covered by some given percentage (often 99%) of the total power of the modulated signal. marker. A value of 100% will cause the entire frequency span to be captured by the OBW marker.
parameter specifies the percentage of total power in the measurementSee the Measurement Method section of the About OBW topic for more information about how OBW is calculated.
See Also