Importing and Exporting Math Functions
Save and recall math functions from the dialog by clicking the or buttons, respectively.
Math functions are saved with the file extension .MTHX. The 89600 VSA can recall math functions with the file extension .MTH (version 12 and earlier) or .MTHX (version 13 and later).
Math functions defined in the dialog are located in the following directory:
%USERPROFILE%\My Documents\Keysight\89600B VSA\MathFunctions
See Also