Auto Frequency Step (Frequency)
If is selected, the VSA automatically calculates the most appropriate Center Frequency Step size for the current configuration. This means a Frequency Step cannot be specified. If is cleared, the step size can be specified.
The frequency step size determines by how much the center frequency is increased or decreased when using the mouse wheel or keyboard arrow keys to change the change the center frequency.
See Also