Paste (Edit)
Click to copy the contents of the clipboard into the currently selected text box, trace hotspot, or marker readout.
When you click , a confirmation dialog will be shown:
When the number on the clipboard is followed by valid units according to the context, the units dropdown will be set accordingly; otherwise the base units are used. If the units are not valid in the current context, a dialog will ask you whether you want to use the number with the base units.
Base units are generally the unit without a quantifier. For example, frequency base units are Hz. Time base units are seconds, etc.
See Also