Save / Recall Display Preferences (Save and Recall)
The appearance of the 89600 VSA user interface is configured in the Display Preferences dialog box (). To make it easy to replicate these settings, and will save and recall all settings in the tabs of the dialog box.
The ability to store display preferences can be used to enhance other Save/Recall functionality (like and by recalling specific visual effects for the measurement.
are saved in a file with the extension .DSPX. The Display Appearance files created by the 89600 VSA software version 12 or lower (.DSP) cannot be recalled by this version of the 89600 VSA.
See Also