About Gate Triggering

The gate trigger allows for control over when and for how long each acquisition is made for each step in performing a stepped spectrum measurement.

Gate Triggering is enabled only for Power Spectrum measurements.

Setting up a Trigger Condition

Gate Trigger setup parameters are located in the Gate Trigger Tab. The parameters shown on the Gate Trigger Tab depend on the Active Input Domain (selected in the Acquisition > Segmented Capture tab).

Gate Trigger Parameters:

See Also

Gate Trigger Tab