Analog Demod Properties Dialog Box

The Analog Demod Properties dialog box provides controls to select the type of analog demodulation to be applied to your signal, as well as other configuration options. The settings available are listed as follows:

The Analog Demod measurement type be selected before AM, PM, or FM demodulation can be selected. To do this, click Analysis > Type > General Purpose > Analog Demod.

See Also

Selecting Analog Demod

Analog Demod Block Diagram

PM Demodulation (Analog Demod)

AM Demodulation (Analog Demod)

FM Demodulation (Analog Demod)

Auto Carrier Frequency/Phase (Analog Demod)