Calibration Mode Auto

Default: selected (enabled)

When Calibration Mode Auto is enabled, the VSA software will use the mode that the native hardware was set to at the time the VSA connected to it. Calibration Mode Auto is only visible and available if the connected instrument supports it.

See Also

About Calibration

User Calibration File Format