SCPI Log Window
When SCPI is enabled, the SCPI Log window appears below the trace windows and shows SCPI commands sent from the VSA software.
The level of information shown in the SCPI Log, and the number of entries, are controlled by settings in the SCPI Preferences tab. If the Logging Level on that tab is set to SCPI Command and Response, the SCPI Log also shows responses to SCPI query commands.
The following illustration is shown with verbose logging selected. You can clear the SCPI Log, select multiple rows, and use a right- click context menu to copy selected rows to the Windows clip board.