Record Toolbar

The record toolbar contains buttons for recording a signal from the selected input.

Record

Begins recording data from the current Analyzer Configuration. Changes measurement data source (Acquisition Menu > Data) to Recording.

See Creating a Recording for more information.

Toggle Data Source Selects between measurement hardware or a recording for the measurement data source.
Disconnect Releases connected hardware from VSA control.

See Also

About Recordings