Math (Trace Data)
trace data displays the results of the selected math function.
Math trace data is available only when a math function is defined. To learn how to create a math function, see Creating Math Functions.
When a math function that cannot be calculated is selected, the VSA shows a grid with no data. If this happens, examine the math function to determine if the math function is correct. Also examine operands in the math function. Some operands, such as data registers, may have no data.
See Also