Raw Repetition Info (IQ-NC)
table shows start time, amplitude, phase offset and delta values between signal repetitions.
Raw Repetition Info is a type of Matrix Table that provides sortable rows by column, selectable column visibility, and copy/paste and export functionality to share rows of content or complete tables to applications like email, text editing or spreadsheet programs.
| Repetition | Start Time (sec) | Amplitude (dB) | Phase Offset (deg) | Δ Start Time (sec) | Δ Amplitude (dB) | Δ Phase Offset (deg) |
|---|---|---|---|---|---|---|
|
Repetition is the index of the repetition. |
is the location of the repetition within the Raw Main Time trace. It is an offset relative to the trigger time. |
is the amplitude difference relative to the first repetition (so the first row will always be 0.00 dB). |
is the difference in phase of each repetition relative to the first (so that the first row will always be 0 degrees). |
is the difference between the next repetition's Start Time and the current repetition's Start time. For example, the Delta Start Time in row 1 shows the time between the start of repetition 2 and repetition 1. The last row will show *** to indicate that the value cannot be computed (no adjacent repetition to compute the difference with). |
is the difference between the next repetition's Start Time and the current repetition's Start time. For example, the Delta Start Time in row 1 shows the time between the start of repetition 2 and repetition 1. The last row will show *** to indicate that the value cannot be computed (no adjacent repetition to compute the difference with). |
is the difference between the next repetition's Start Time and the current repetition's Start time. For example, the Delta Start Time in row 1 shows the time between the start of repetition 2 and repetition 1. The last row will show *** to indicate that the value cannot be computed (no adjacent repetition to compute the difference with). |
See Also