Segmented Main Time

Shows all segments of time data.

Segmented Main Time does not support Time averaging (Analysis > Average) or any other average types. However, it does support trace averaging (Trace > Properties > Average).

Segmented Main Time draws segment separator lines on the first point of a segment, except when zoomed to within a single segment. When the start and stop times are both within the same segment, the regular grid is shown (10 vertical divisions).

The trace also supports two different display modes: Condensed and Overlapped. For details, see Time Segment Display Mode.

To see data only from the selected segment, use the Spectrum and Main Time traces (Analysis > Time).