RF Center Frequency (User Correction)

Menu Path: Acquisition > User Correction

The RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). center frequency for the external downconverter can be entered in this text box. The VSA center frequency defaults to this value when Frequency Converter is selected. (The VSA center frequency can still be changed within the frequency band defined by the external downconverter center frequency ± ½ the External Bandwidth specified.)

When Frequency Converter is selected, the displayed measurement center frequency is the RF Center Frequency rather than the measurement hardware center frequency.

See Also

Frequency Converter