Domain (Units Tab)
selects the frequency domain or time domain. Since limit lines can only be applied to frequency or time-domain data, is used to verify that a limit test is applied to an applicable trace. A status error will appear if the trace is not applicable. also determines the appropriate X-axis and Y-axis units.
See Also