Eq Impulse Response (802.15.4 HRP UWB)
shows the 802.15.4 HRP UWB signal's impulse response, which is computed from the SYNC portion of the SHR. Eq Impulse Response is averaged over all repetitions of the Si symbol, except for the first and last repetition. The number of averaged Si symbols is shown above the trace in the Vect: NN annotation, where NN is the number of averages.
See Also