License Mappings

The VSA software currently supports 89601C feature licenses as well as legacy licenses (e.g., 89601B). The following table illustrates the mapping between 89601C feature licenses and equivalent legacy 89601B option licenses.

Name 89601C Feature Legacy 89601B Options Measurement Modes/Description
Direct Data Connectivity 89601101C --- Direct (user input) streaming of data without connected hardware
Basic Vector Analysis 89601200C 200 + BHL (CQM) Vector, Analog Demod, Component Test, Power Spectrum
Basic Vector Analysis - Advanced 89601201C --- Vector, Analog Demod, Component Test, Power Spectrum - (tiered licensing, Advanced)
Basic Vector Analysis - Upgrade from Standard to Advanced 89601201U --- Vector, Analog Demod, Component Test, Power Spectrum - (tiered licensing, Upgrade from Standard to Advanced)
Basic Vector Analysis - Standard 89601202C --- Vector, Analog Demod, Component Test, Power Spectrum - (tiered licensing, Standard)
Basic Vector Analysis - Upgrade from Essentials to Standard 89601202U --- Vector, Analog Demod, Component Test, Power Spectrum - (tiered licensing, Upgrade from Essentials to Standard)
Basic Vector Analysis - Essentials 89601203C --- Vector, Analog Demod, Component Test, Power Spectrum - (tiered licensing, Essentials)
Multi-vendor Hardware Connectivity 89601301C 301 Multi-vendor hardware
Digital Demodulation Analysis 89601AYAC AYA + BHK (CustomIQ) + BHA (TEDS) Digital Demod, TEDS, Custom IQ, GSM Global System for Mobile Communications: Originally developed as a pan-European standard for digital mobile telephony, GSM has become the world’s most widely used mobile system. It is used on the 900 MHz and 1800 MHz frequencies in Europe, Asia and Australia, and the 1900 MHz frequency in North America and Latin America./EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.)/EDGE Evo, Flex Frame
3GPP Modulation Analysis 89601B7NC B7N (B7T + B7U + B7W + B7X) cdma2000, WCDMA, 1xEV-DO, TD-SCDMA
Wireless Connectivity Modulation Analysis 89601B7RC B7R (11abgjp) + B7Y (WiMax) 802.11a/g/j/p OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS., 802.11b/g DSSS Direct sequence spread spectrum. The data transmission scheme (sometimes referred to as a "'modulation" scheme) used in 802.11b WLANs. DSSS uses a radio transmitter operating at a fixed centre frequency, but using a relatively broad range of frequencies, to spread data transmissions over a fixed range of the frequency band. 802.11a and 802.11g (when not operating in 802.11b mode) use Orthogonal Frequency Division Multiplexing (OFDM)., 802.16 OFDM, 802.16 OFDMA
Custom OFDM Modulation Analysis 89601BHFC BHF Custom OFDM
LTE/LTE-A FDD Frequency Division Duplex: A duplex scheme in which uplink and downlink transmissions use different frequencies but are typically simultaneous. Modulation Analysis 89601BHGC BHD (LTE FDD) + BHG (LTA-A FDD) LTE/LTE-A (FDD)
LTE/LTE-A TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period. Modulation Analysis 89601BHHC BHE (LTE TDD) + BHH (LTE-A TDD) LTE/LTE-A (TDD)
DOCSIS Modulation Analysis 89601BHMC BHM Docsis 3.1 Upstream, Docsis 3.1 Downstream
5G NR Modulation Analysis 89601BHNC BHN 5G NR, Pre-5G
FMCW Radar Analysis 89601BHPC BHP FMCW Radar
Pulse Analysis 89601BHQC BHQ Pulse, Advanced Radar
IoT Modulation Analysis 89601BHTC BHC (RFID) + BHT (NB-IoT) NB-IoT, RFID, 802.15.4 HRP UWB (89601BHTC only)
High Throughput WLAN WLAN - Wireless Local Area Network: A system that includes the distribution system (DS), access points (APs), and portal entities. It is also the logical location of distribution and integration service functions of an extended service set (ESS). A WLAN system contains one or more APs and zero or more portals in addition to the DS. Modulation Analysis 89601BHXC, 89601BVXC BHJ (11n/ac) + BHX (11ax) 802.11n/ac/ax
Phase Coherent Channel Count Expander up to 8 Ports 89601CC1C --- Phase coherency up to 8 ports
Phase Coherent Channel Count Expander up to 64 Ports 89601CC2C --- Phase coherency up to 64 ports
Channel Sounding Measurement 89601CSDC --- Channel Sounding
DVB Satellite Communications Analysis 89601DVBC --- DVB-S2X, DVB-RCS2
Cross-Correlated EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. and IQ-NC 89601EVMC --- Enhanced EVM Analysis with ccEVM and IQ-NC
5G NR EVM Metric 89601OR1C --- 5G NR EVM metric
5G NR BLER Block Error Rate - A ratio of the number of erroneous blocks to the total number of blocks received on a digital circuit. Block error rate (BLER) is used for W-CDMA performance requirements tests (demodulation tests in multipath conditions, etc). BLER is measured after channel de-interleaving and decoding by evaluating the Cyclic Redundancy Check (CRC) on each transport block. Metric 89601OR2C --- 5G NR BLER metric
Power Suite 89601PSMC --- Adjacent Channel Power, Spectral Emissions Mask
ORAN Uplink Performance Improvement 89601ULPC --- ORAN Uplink Performance Improvement for 5G NR (requires 89601BHNC)
Flex Frame Signal Generation 89602AYAC --- Generate, save, recall and download Flex Frame signals
DVB Satellite Communication Signal Generation 89602DVBC --- Generate, save, recall and download DVB-S2/S2X and DVB-RCS2 signals

See Also

License Dialog Box

Optional Measurement Software