Decode Tab (LTE-Advanced)
Menu Path: where x specifies the component carrier
The tab of the LTE-Advanced Demod Properties dialog box allows you to specify what level of channel decoding to perform as well as specify other parameters needed for information decoding for the DL Decode Info and UL Decode Info summary tables. The decoded bits are shown on the Decoded Symbol Table (uplink) and the CW 0/1 Decoded Symbol Tables (downlink).
At the top of this tab there is a set of buttons for selecting which component carrier to configure. The selected component carrier (x) is indicated by the green button and by the text "CCx" in the tab title.
There are two different versions of the tab, one for downlink and one for uplink signals.
Downlink parameters
The parameters for the downlink version of the tab are listed below (click on a parameter for more information).
-
Decoded Symbol Table Results
-
The PDSCH Bits selection is only enabled when RB Auto Detect Mode is set to .
- CRC Decode Max Iteration Count
- DCI Formats 1/1A Detection Include
- Transmission Modes to include in DCI decoding
- Uplink Bandwidth
-
RNTI Ranges (User Defined)
- Latest PMI Precoding Matrix Indicator Report on PUSCH Physical Uplink Shared Channel
Uplink parameters
The parameters for the uplink version of the tab are listed below (click on a parameter for more information).
- Decoded Symbol Table Results
- CRC Decode Max Iteration Count
-
- HARQ-ACK
- CQI/PMI
- TDD Ack/Nack Feedback Mode
See Also