P-SS/S-SS Antenna Port (LTE-Advanced)
Port 0
Port 0, Port 1, Port 2, Port 3, All Port
C-RS Cell-specific RS antenna port(s) that P-SS and S-SS are transmitted on. P-SS Primary Synchronization Signal and S-SS Secondary Synchronization Signal can be transmitted on a single antenna port or all the C-RS antenna ports at once.
specifies theWhen Basic Tab (Downlink Control Channel Properties) is assumed to be split equally among the transmit antennas.
is selected, the value for P-SS and S-SS entered in theFor example, when P-SS
= 0.6 dB and is set to for a signal with four C-RS antenna ports, the demodulator will expect P-SS power on each antenna port to be 0.6 dB - 6.02 dB = -5.38 dB.Otherwise, when
, , , or is selected, the entire power specified by the P-SS and S-SS parameter is assumed to be transmitted on the selected antenna port.See Also