RB Auto Detect (LTE-Advanced)
Selected
enables autodetection of user allocations.
For downlink, the demodulator can perform power based autodetection or can autodetect allocations by decoding PDCCH Physical Downlink Control Channel. See the RB Auto Detect Mode for more information.
For uplink, PUSCH Physical Uplink Shared Channel, PUCCH Physical Uplink Control Channel, SRS Signaling Reference Signal, and PRACH Physical Random Access Channel allocations can be autodetected when the required Channel or Signal Parameters are specified in the LTE Allocation Editor for each channel.
See the LTE Allocation Editor and Setting Up User Allocations topics for more information.
For uplink signals, the LTE Long Term Evolution-Advanced demodulator can perform sync slot autodetection or user-assisted autodetection.
To configure automatic sync slot detection, select the parameter on the PUSCH tab or PUCCH tab in the LTE Allocation Editor.
To configure user-assisted autodetection, clear the parameter for a channel and define a sync slot with associated (in the LTE Allocation Editor) to be used for initial synchronization. User-assisted auto-detection results in faster measurements than automatic sync slot detection.
See Also