PRACH allocations (LTE-Advanced)
To configure a PRACH Physical Random Access Channel channel, follow these steps:
-
Select the tab (on the left)
PRACH cannot be analyzed simultaneously with PUSCH Physical Uplink Shared Channel, PUCCH Physical Uplink Control Channel, and SRS Signaling Reference Signal.
- Set
- Return to Uplink user allocations and configure another type of channel or signal.
For more information about the parameters, see the LTE Allocation Editor topic.
See Also