EVM Pk (LTE-Advanced)
shows the signal's peak EVM value and location (symbol and subcarrier) within the frame. Only channels and signals that are selected for analysis in the Composite Include list on the , except , are included in the EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. peak search.
See EVM topic in the for more information about EVM calculations.
can also be shown in units of dB by selecting the Report EVM in dB parameter.
See Also