RSPwr (LTE-Advanced)
shows the average power of the cell-specific reference signal from a C-RS Cell-specific RS/Rx path.
is expressed in dB relative to the power of C-RS on the reference C-RS/Rx path and is calculated from the data in the Measurement Interval.
See Also