Freq Err Per Slot (LTE-Advanced)
shows the frequency error of the signal as a function of slot number for the data in the Measurement Interval. This is the frequency error that is compensated on a per-slot basis as part of the EVM minimization process.
The frequency error is expressed as an offset in Hz from the center frequency of component carrier x (CC center frequency = VSA center frequency + CC Frequency Offset).
See Also