MustUsern IQ Meas (LTE-Advanced)
shows the IQ values for MUST user channels/signals in the selected layer.
The trace is only available for downlink and when MUST is selected as the Multiple Access scheme.
See IQ Meas for more information on IQ Measurement traces.
See Also