Search Time (LTE-Advanced)
shows the time record data after resampling and time adjustment. The beginning of the trace is set to the trigger location (which corresponds to 0 ms in Raw Main Time), and the time scale of is shifted such that 0 ms corresponds to the beginning of the LTE Long Term Evolution-Advanced frame. Note that the beginning of the frame does not actually have to be in .
The next step is to locate the Measurement Interval in the data and place the data into the Time trace.
See Also