Spectrum (LTE-Advanced)
shows the frequency spectrum of the pre-demodulated trace data.
When averaging is , and Inst Spectrum are identical, but when averaging is turned on, will display an averaged frequency spectrum (will still show the frequency spectrum of the current measurement).
See the Spectrum trace topic in the Reference for more information.
See Also