Result Length (LTE)
20 slots or the length of the signal, whichever is larger
Measurement Interval and Measurement Offset specify which part of the time capture is demodulated.
determines how many slots will be available for demodulation.The result data starts where the analysis boundary is found and ends after the amount of data specified by .
The length of the time capture (contained in Search Time) is longer than the result length by approximately the length of the Analysis Start Boundary (frame = 10 ms, slot = 0.5 ms, etc.) to allow for location of the analysis boundary within the time capture.
For downlink, an entire slot containing S-SS Secondary Synchronization Signal must be present in the time capture (Raw Main Time) for demodulation to occur.
See Also