UL Spectrum Flatness (LTE)
The parameters for are used to calculate the limit lines that are automatically added to the In-band Emissions trace.
See Section 6.5.2.4 of TS Technical Specification 36.521-1 for more information about spectrum flatness requirements.
Channel Condition
Specifies which set of requirements the limit lines are based on. Possible selections are and .
Frequency band
The limits specified by the standard depend on the width of the frequency band containing the LTE Long Term Evolution signal and the location of the LTE frame within the band. This information is specified by the following parameters:
- : specifies the center of the LTE frame within the frequency band determined by FUL Up Link (reverse link: from cell phone to base station) LOW and FUL HIGH.
- : specifies the lower band edge.
- : specifies the upper band edge.
There is no dependency between these parameters and the VSA's center frequency.
See Also