In-band Emissions Result (LTE)
Menu Path:
shows the results of the auto-generated limit test on the In-band Emissions trace. This includes PASS/FAIL status as well as the location of the highest point in the trace along with the delta from the limit. For a PASS result, this delta value is the Narrowest Pass Margin. For a FAIL result, this delta value is the Widest Fail Margin.
This information is also shown in the Markers window.
See Also