PUSCH (LTE)
PUSCH Physical Uplink Shared Channel (Physical Uplink Shared Channel) contains uplink user data.
When is selected, Frame Summary will show a PUSCH group named for each modulation type under .
When is cleared, will show the PUSCH information in the row for the uplink user currently selected for analysis. The other user's rows will show "---" since the demodulator can only analyze one user at a time.
Uplink user allocations can be defined in the LTE Allocation Editor.
This channel's SC-FDMA Single Carrier - Frequency Division Multiple Access modulation type will be displayed as QPSK Quadrature phase shift keying, 16QAM, or 64QAM when the PUSCH channel contains a single modulation type. When PUSCH contains a combination of modulation types, will display "---".
See Also