Importing and Exporting Macros

You can import and export macros by using the Import and Export buttons on the Macros Dialog Tab.

Macros are no longer contained in one file (as in versions of the 89600 VSA earlier than 13.00) but are a complete Visual Studio solution. When you click the Import button, you will need to browse to the directory that contains the .SLN file for the macro.

Imported macros are copied to the following directory:

%USERPROFILE%\My Documents\Keysight\89600B VSA\Macros

See Also

About Macros

Creating a Macro