About the Macros Window
The Macros dialog). To start and run a macro, click the run button.
tool window is used to easily run one or more VSA macros. The window contains a run button for each currently defined macro (a list of maco's are listed in theAny currently running macros will be disabled until the running macro exits.
To view the .NET API 1) Access Preamble Indicator, or 2) Application Programming Interface command code associated with each VSA GUI operation (selection), open the Output Window and select the property.
See Also