Stopping a Macro
A currently executing macro can be stopped by selecting the macro in the dialog and clicking the button.
Clicking the Run button always runs the macro starting with the first line of code. If you click the button and then click the button, execution begins from the first line of code, not from where the macro stopped.
The macro thread will be ended as soon as the button is pressed and the macro code will not be given a chance to do any cleanup.
See Also