Error Summary Table (MB-OFDM)
Menu Path:
The Composite Error Summary table provides measurement and analysis information unique to the MB-OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Composite Error Summary trace data and MB-OFDM modulation analysis. A list of the available error data is provided in the Available Data Results topic, which also links to detailed descriptions for each error result.
See Also
Available Error Summary Data (MB-OFDM)
Available Band Errors Summary Data (MB-OFDM)