Preamble Correlation (MB-OFDM)
is the correlation between the measured preamble and an ideal preamble. It represents an indication of the quality of the preamble. is displayed as a symbol by symbol correlation of the entire preamble [PS physical slot: A unit of time, dependent on the PHY specification, for allocating bandwidth. 802.11: Power save (mode)/FS fixed subscriber: A subscriber station that does not support communications whilst in motion. (Sync) and CE (Channel Estimation) portions]. This trace can be used to look at problems with the scalar correlation values as seen on the Composite .
See Also
Available Trace Data (MB-OFDM)