IQ Ref Time (NB-IoT)
shows the same information as the IQ Ref trace when the data is shown in the or trace format. When the data is shown in any other format, time is on the horizontal axis instead of frequency as in the trace.
The information in the IQ Ref topic applies to , with the exception mentioned above.
See Also